Technical FAQs

Ask a Question

What is the maximum number of master cartridges that can be used on an 8501XO relay?

A maximum of six master cartridges may be used on any 7 and 8 pole AC relay. Do not use any master cartridges on a 9 - 12 pole AC relay or any DC controlled relay.

CTA-ID : 2051801
Was this helpful?
What can we do to improve the information ?