Technical FAQs

Ask a Question

Are Short Circuit Current Ratings printed on the nameplate of factory assembled NQ, NF, or I-Line panelboards?

Issue:

Are Short Circuit Current Ratings printed on the nameplate of factory assembled  NQ, NF, or I-Line panelboards?

 

Product Line:

Panelboards

 

Environment:

Standards

 

Cause:

Features

 

Resolution:

No. AIC or SCCR ratings are never printed on the nameplate of a panelboard, since later installation of different breakers could change the overall AIC/SCCR  rating.. Label for Series ratings is located in the hardware bag and can be attached to trim by Customer , with space available for Customer's current Panel's SCCR rating . Individual AIC ratings are labeled on individual breakers


CTA-ID : 2051711

Was this helpful?
What can we do to improve the information ?