Technical FAQs

Ask a Question

What is the difference between the interior trim kits MH53UTK and MH534TK?

Issue:
What is the difference between the interior trim kits MH53UTK and MH534TK?

Product Line:
PTFDS - FD Enclosure Systems

Environment:
Panelboard enclosures sold and supported in the USA.

Cause:
Differentiation between MH534TK and MH53UTK.

Resolution:
The MH53UTK is for use with the enclosure that is put together with screws and the MH534TK is for use with the enclosure that is welded together.  This is indicated by the Series of the enclosure.
The MH53UTK is for the Series E2 enclosure, the MH534TK is for the Series E1 enclosure.  









CTA-ID : 2051284
Was this helpful?
What can we do to improve the information ?