Technical FAQs

Ask a Question

What are the repair parts for a QO14060L200GRB, Series S02, Load Center?

Issue:
Current design repair parts

Product line:
QO load centers

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable.
Cover - 4056317450  
Interior trim with Labels - 4056313901K
Interior Assembly - QO14060L200GRBI
Neutral bonding screw - 4028344850K
Main Lugs - QOL225
Outdoor cover latch - 4056314701
Latch rivet - 2410212160
Interior trim mounting screw - 4020513001K
RB door mounting screws - 2142217101
Main circuit breaker and main lugs keps nut - 2342702001


CTA-ID : 2051234
Was this helpful?
What can we do to improve the information ?