Technical FAQs

Ask a Question

What is the kVA range of the Mini Power Zone (MPZ and MPZB) product line?

MPZ that SENA offers range from 15- 30KVA 3 phase and 5 - 25 kVA 1 Phase. If a larger unit is required an IPaCs product is recommended.
For more information
Contact IPaCS
Main Telephone: 704-637-9662
IPaCS Address: 105 Summit Park Drive - Salisbury, NC 28146

CTA-ID : 2051886
Was this helpful?
What can we do to improve the information ?