Technical FAQs

Ask a Question

QO70AN Wire Range

Issue:
What is the wire range of the QO70AN lug?

Product Line:
QO load centers and accessories sold and supported in the USA.

Environment:
Application

Cause:
Determining the correct wire size for a QO70AN lug.

Resolution:
The QO70AN accepts #10 to #2 aluminum or #14 to #4 Copper.


CTA-ID : 2051829
Was this helpful?
What can we do to improve the information ?