Technical FAQs

Ask a Question

What are the repair parts for a QO14060L200G, Series S1, Load Center?

Issue:
Current design repair parts

Product Line:
QO load centers

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are concidered field replaceable.
Cover - QOC40UF/S
Interior Assembly - QO14060L200GI
Neutral bonding screw - 4028344850K
Main Lugs - QOL225
Indoor cover mounting screw - 4020513002K
Indoor cover door hinge - 4028356450K (Kit contains parts to repair one hinge)
Door Latch Kit - 4020284450K
Main circuit breaker and main lugs keps nut - 2342702001


CTA-ID : 2051222
Was this helpful?
What can we do to improve the information ?