Technical FAQs

Ask a Question

What NEMA types of enclosures are available for QO load centers?

Issue:
Product Features

Product Line:
QO load centers

Environment:
Enclosure Types

Cause:
Application

Resolution:
The QO load centers are available in Nema type 1(indoor) and Nema type 3R(Outdoor) enclosures only.


CTA-ID : 2051321
Was this helpful?
What can we do to improve the information ?