Technical FAQs

Ask a Question

What input voltage can be applied to a RC87610240 counter?

Issue:
What input voltage can be applied to a RC87610240 counter?

Product Line:
Zelio Counters

Environment:
All products

Cause:
Device Wiring

Resolution:
The input to the counter is: 5-50 VDC or VAC on terminals 2 and 3. Or, 48-240V AC only on pins 1 and 2.


CTA-ID : 2051901
Was this helpful?
What can we do to improve the information ?