Technical FAQs

Ask a Question

Is the QO3125SL UL listed? What is the UL File number?

Yes, it is in UL File E92411, Volume 1, Section 4.


CTA-ID : 2051878
Was this helpful?
What can we do to improve the information ?