Technical FAQs

Ask a Question

Specification requires that ``cooling fans, if required, shall incorporate anti-friction bearings and internal impedance type motor protection``. Please advise whether the standard cooling fans that Seneca provides meet this requirement.

Yes, our cooling fans meet the specifications.


CTA-ID : 2051923
Was this helpful?
What can we do to improve the information ?