Technical FAQs

Ask a Question

Customer is ordering 7-section MCC and they are only using the first 5 sections initially. Can they order a temporary cover for the end of section 5?

Need to order part # 80450-430-56. When the customer gets ready to splice sections 6 and 7 to the line-up, they can remove the right sideplate from section 5 and discard.

CTA-ID : 2051921
Was this helpful?
What can we do to improve the information ?