Technical FAQs

Ask a Question

What is the UL file number for the Powerpact D frame (and Compact NSJ) lugs?

The lugs in the 32508 and 32510 kit are in UL file E63335SP, Vol. 3, Sec. 2.


CTA-ID : 2051793
Was this helpful?
What can we do to improve the information ?