Technical FAQs

Ask a Question

The Instructions for the GJL36007M02 Mag-Gard breaker shows 2-minimums and 2-maximums on the adjustment dial and I need help understanding this.

The Mag-Loc adjustment range limiter allows a user to limit the adjustment of the instantaneous trip setting within the range of 3-11 times the rated current. Once the range has been set, replace the cover and install a cover seal to prevent tampering. This feature allows adjustment within a predefined, customized range of short-circuit protection. With the Mag-Loc ring and cover on the breaker you are limited to part of the adjustment range. The Installer sets the ring which limits the adjustment to that part of the range.

CTA-ID : 2051734
Was this helpful?
What can we do to improve the information ?