Technical FAQs

Ask a Question

What is the part number for a Model 5 100a breaker stab assembly ?.

Issue:
Replacement Part/s

Product Line:
MCC5

Environment:
Branch breaker or Starter breaker

Cause:
Worn part

Resolution:
Stab will only fit a F frame breaker up to 100 amps, quantity 3 will be needed, part number will be 40555-041-51
Also consider a stab shroud 40555-003-01 , line shroud 40555-004-01, 8 rivets 24303-63280 and a 2 oz joint compound PJC7201

CTA-ID : 2051729
Was this helpful?
What can we do to improve the information ?