Technical FAQs

Ask a Question

What are the number of operations for a metalclad breaker?

The number of full load current switching operations is 10,000. The number of no load operations is also 10,000. The exception is the 50kA breaker which has 5000 full load current switching operations.

CTA-ID : 2050971
Was this helpful?
What can we do to improve the information ?