Technical FAQs

Ask a Question

What is the replacement for a line isolation monitor part number 43134-007-50?

Issue:
What is the replacement for a line isolation monitor, part number 43134-007-50?

Product Line:
Hospital Isolation Equipment

Environment:
Cross Reference/replacement

Cause:
Replacement of obsolete monitor

Resolution:
"IGD`` was  the part number for the  line isolation monitor; however, that is now obsolete, replaced by the current IG6M.  However, this is the monitor only, other components may be required depending on what type of annunciator is being used.  See MED10130101 on the Technical Library for further component identification.
Was this helpful?
What can we do to improve the information ?