Technical FAQs

Ask a Question

Does an energy efficient transformer have to be de-energized to install a weathershield?

ABSOLUTELY!! Whenever work is being done on an electrical device, the power to the device needs to be turned off. In this case, the front and rear panel need to be partially removed since the weathershield and the front/rear panels share mounting bolts.

CTA-ID : 2050990
Was this helpful?
What can we do to improve the information ?