Technical FAQs

Ask a Question

Is the handle only available for the XD4PA** or XD5PA** ?<br /><br />

The operator only is available.
ZD4PA12 is 2 direction maintained ZD5PA12 is 2 direction maintained
ZD4PA22 is 2 direction spring return ZD5PA22 is 2 direction spring return
ZD4PA14 is 4 direction maintained ZD5PA14 is 4 direction maintained
ZD4PA24 is 4 direction spring return ZD5PA24 is 4 direction spring return



CTA-ID : 2051722
Was this helpful?
What can we do to improve the information ?