Technical FAQs

Ask a Question

What is difference between surface and flush trims for load centers?

Surface trims come even with the edge of the boxes and flush trims will overlap the load center enclosure by .60`` (19/32``) on all sides to create a nice transition to finished wall.


CTA-ID : 2051698
Was this helpful?
What can we do to improve the information ?