Technical FAQs

Ask a Question

What is the replacement interior for a H364 series E2?

Not available as complete interior, need to order the line base assembly, part number 40560-282-50, and the load base assembly part number 40560-281-50 (OBSOLETE - NO REPLACEMENT) and lug assembly if needed is part number 40251-162-51.

CTA-ID : 2051212
Was this helpful?
What can we do to improve the information ?