Technical FAQs

Ask a Question

What is the replacement external reset mechanism for an 8738SBW in a Nema 4X stainless steel enclosure?

The parts would be:
Qty 1 - 30019-113-56 Reset sub-assembly (does not include the ring nut or gasket listed below).
Qty 1 - 30019-121-01 Ring nut.
Qty 1 - 9066 W1 Protective boot (also serves as gasket) (required on NEMA Type 4/4X enclosures).


CTA-ID : 2051915
Was this helpful?
What can we do to improve the information ?