Technical FAQs

Ask a Question

What is the information on the battery used in the RC87610050 Counter?<br />

The cell size reference is 1/2 R6 - 1/2 AA. This is the LS14250 - 3.6v primary lithium - thionyl chloride (Li-SOCl2) high drain 1/2 AA - size cell. It is 14.5mm (0.57 inches) diameter and 24.8mm (0.98 inches) height.


CTA-ID : 2051913
Was this helpful?
What can we do to improve the information ?