Technical FAQs

Ask a Question

When series rating EZM main circuit breakers, how can EZM11000CBU and EZM11200CBU main breaker sections be rated at 100K AIC when the MH main breaker they use are rated at only 65K?

For these Ampere ratings only, these EZM main devices EZM11000CBU and EZM11200CBU come with a factory installed specially rated MHF type breakers that are listed and tested up to 100k at 240V maximum SCCR and can be series rated as shown on page 2-9, table 2.12 in digest 175.

CTA-ID : 2051550
Was this helpful?
What can we do to improve the information ?