Technical FAQs

Ask a Question

<br />Wanting to know if the 6`` cover plate comes with the door hinges.

Told him yes that the 6`` and up to 24`` would have the door hinges.


CTA-ID : 2051535
Was this helpful?
What can we do to improve the information ?