Technical FAQs

Ask a Question

What is the terminal data for the NF125SFL?

Issue:
What is the wire size for the NF125SFL?

Product Line:
NF Panelboards

Environment:
Installation 

Cause:
Product Features 

Resolution:
The wire size is (2) #6 to 2/0 Al or Cu wire per lug.

CTA-ID : 2051396
Was this helpful?
What can we do to improve the information ?