Technical FAQs

Ask a Question

What is the maximum wire size for a 1200a RGA breaker with aluminum wiring ?

The lugs are AL1200R53K rated for (4) 3/0-600kcmil max Al or Cu


CTA-ID : 2051394
Was this helpful?
What can we do to improve the information ?