Technical FAQs

Ask a Question

What is the Pressure setting or J Code value for a 9013FSG2J20

Pressure switch closes at 20 PSI and opens at 40 PSI. See Digest 175, page 22-19 Table 22.50.


CTA-ID : 2051646
Was this helpful?
What can we do to improve the information ?