Technical FAQs

Ask a Question

Is a retaining means required for a backfed breaker in a load center when used in a photovoltaic application?

Issue:
Product use and installation


Product Line:
QO and Homeline load centers


Cause:
Application

Resolution:

THIS QUESTION REALLY REQUIRES THE INSTALLER TO FOLLOW WHAT THE NATIONAL ELECTRICAL CODE REQUIRES AND OR THE LOCAL CODE AUTHORITY HAVING JURISDICTION.





CTA-ID : 2051701
Was this helpful?
What can we do to improve the information ?