Technical FAQs

Ask a Question

REVISION TO FAQ 2026048: CORRECT SPELLING<br /><br />What is the height of the operating handle for HVL switchgear?

5/15kV - The centerline of the handle mechanism is 54`` above the floor for upright switches. Add 4`` for NEMA 3R base channel.
For inverted switches the centerline of the handle mechanism is 45`` above the floor. Add 4`` for NEMA 3R base channel. NOTE: The handle travel range in 20`` up and 20`` down.
Note for Outdoor units, the operator can stand on the floor above the base channel to operate the switch.


CTA-ID : 2051425
Was this helpful?
What can we do to improve the information ?