Technical FAQs

Ask a Question

What is included in a HOM20M100CBP2?

It includes (1) - HOM20M100C Homeline 100A 20 space / 20 circuit maximum, main breaker load center. (5) - HOM115 Homeline 15A single-pole circuit breakers, and (1) - HOM230 Homeline 30A double-pole circuit breakers.


CTA-ID : 2051480
Was this helpful?
What can we do to improve the information ?