Technical FAQs

Ask a Question

Can I get a three phase 1200A fusible switch main disconnect for the EZM lineup?

No three phase 1200A fusible switch is currently unavailable. They are only available up to 800A. Recommend using an EZM31200CB type circuit breaker disconnect instead.


CTA-ID : 2051193
Was this helpful?
What can we do to improve the information ?