Technical FAQs

Ask a Question

What is the part number for the support brackets included with the QMB1BLW filler plate?

There are two brackets, one for the left side and one for the right side. Order (1) 80100-134-01 and (1) 80100-134-02

CTA-ID : 2051850
Was this helpful?
What can we do to improve the information ?