Technical FAQs

Ask a Question

Which termination options for Powerpact H and J circuit breakers qualify for 100% ratings?

The following termination options may be ordered with 100% ratings: L, F, M, P, S.
The following termination options do not have a 100% rating option: A, N, D, K


CTA-ID : 2051384
Was this helpful?
What can we do to improve the information ?