Technical FAQs

Ask a Question

Is the pilot light bulb included on a XY2CE device?

Identifying whether or not the pilot light is included with an XY2CE cable pull switch

Product Line:
PREVENTA Safety Products

Products sold and used in the United States

Pilot light bulb needed for use with an XY2CE switch

Pilot lights are only available on 2 Normally Open (N.O.) - Normally Closed (N.C.) devices. The bulbs were not included on the older devices that utilized incandescent style bulbs so the bulb was orderedseperately based on voltage. The current line includes a 24-120V LED, if the part number is changed so the 6 becomes a 7 then a 277V light module is included instead.

CTA-ID : 2051551
Was this helpful?
What can we do to improve the information ?