Technical FAQs

Ask a Question

Can the heads be interchanged on the manual reset devices like the XCDR2110N12 OsiSense limit switch?<br /><br />

No. On the manual reset devices, the heads are fixed and cannot be interchanged, unlike the other devices in this product line.


CTA-ID : 2051501
Was this helpful?
What can we do to improve the information ?