Technical FAQs

Ask a Question

What is included in a HOM2040M200VP?

Product design features

Product Line:
Homeline load centers

It consists of a HOM2040M200TC 20 space 40 circuit with factory installed QOM2200VH main breaker load center with equipment ground bar, (3) HOM120 single pole 20Amp and (2) HOM230 two pole 30Amp circuit breakers.

Note: This catalog number is Pending Obsolescence and the Replacement is HOM2040M200PCVP

CTA-ID : 2051475
Was this helpful?
What can we do to improve the information ?