Technical FAQs

Ask a Question

8536SCW13 - is this stainless steel enclosure lockable?<br /><br />

Not as standard. However, factory modification Form G19 will provide a stainless steel hasp to a stainless steel enclosure on NEMA Size 0-5 only. This allows the enclosure door to be padlocked with one standard size padlock.


CTA-ID : 2051423
Was this helpful?
What can we do to improve the information ?