Technical FAQs

Ask a Question

<br />What is the voltage rating on a 9013FHG pressure switch?

The 9013FHG device contacts are horsepower rated, with a control circuit rating of A600. For specific information, see page 22-18, Table 22.49 of Digest 175.

CTA-ID : 2051653
Was this helpful?
What can we do to improve the information ?