Technical FAQs

Ask a Question

On the ATV71 VFD, can you put in a encoder interface card, a controller inside card and an Ethernet IP card in at the same time?

With ATV71 you can connect encoder interface card and more 2 option cards, but you have to take care because some conditions are NOT POSSIBLE:
- 2 communication cards are NOT POSSIBLE;
- 2 times the same option card are NOT POSSIBLE.

Controller Inside is consider as a PLC card and NOT as a communication card.

Some examples of possible configurations:

Example 1
- 1 Communication card (DeviceNet, Ethernet, Profibus or other);
- 1 Encoder Interface Card;
- 1 Controller Inside Card.

Example 2
- 1 Communication card (DeviceNet, Ethernet, Profibus or other);
- 1 Encoder Interface Card;
- 1 Extension I/O Card;



CTA-ID : 2051471
Was this helpful?
What can we do to improve the information ?