Technical FAQs

Ask a Question

What is included in a QO32M100VP?

Issue:
Product design features

Product Line:
Homeline load centers

Resolution:
It consists of a QO132M100C 32 space with a factory installed QOM100VH main breaker load center, (3) QO120 single pole 20Amp circuit breakers and (2) QO230 2 pole 30Amp circuit breaker.


CTA-ID : 2051462
Was this helpful?
What can we do to improve the information ?