Technical FAQs

Ask a Question

What is included in a QO3040M200VP?

Product design features

Product Line:
Homeline load centers

(1) QO13040M200C 30 space, 40 circuit, load center with a factory installed QOM2200VH main breaker.
(3) QO120 circuit breakers
(2) QO230 circuit breakers

CTA-ID : 2051453
Was this helpful?
What can we do to improve the information ?