Technical FAQs

Ask a Question

What is the difference between 9007C52N2 and 9007C52N?<br /><br />

Deleting the 2 from the Type number makes it factory set for CW operation only. This is a procedure that can be completed in the field, and can be reversed to return to CW and CCW operation, if desired.

CTA-ID : 2051452
Was this helpful?
What can we do to improve the information ?