Technical FAQs

Ask a Question

Can Schneider Electric HVL switches be built in a 42" wide section? This is an outdoor NEMA 3R application retrofit job. Existing is S&C which is 42" wide.

No Schneider Electric will not build the HVL switch in a 42" section, but Schneider Electric can use 3" NEMA 3R collars to correct some of the distances. TAG #58 was created for the 3" NEMA 3R collar.


CTA-ID : 2051430
Was this helpful?
What can we do to improve the information ?