Technical FAQs

Ask a Question

What size is the switch/fuse viewing window for the 5/15kV HVL switch enclosure? How high is it from the floor?

The viewing window is 5.5" high and 21.5" wide. The center line of the window is 67.5" from the floor for indoor. Add 4" for NEMA 3R base channel.

For inverted switches the center line of the window is 41" from the floor for indoor. Add 4" for NEMA 3R base channel.

Revised 01/14/09.

CTA-ID : 2051427
Was this helpful?
What can we do to improve the information ?