Technical FAQs

Ask a Question

What is the Nema rating for 9001K52 and 9001K51 closing plate?

Closing plates meet Nema 1, 2, 3, 4, 4 X, 6, 12 and 13 ratings. They are made of plastic with the 9001K51 being grey and the 9001K52 being black plastic.

CTA-ID : 2051350
Was this helpful?
What can we do to improve the information ?