Technical FAQs

Ask a Question

Do the GS1and LK3 switches meet the NFPA 79 standards?

Yes for GS1 devices up to 400A and LK3 devices up to 200A. They also need an internal handle, use GS1AD010 for 5x5 shafts or GS1AD020 for 10x10 shafts.

CTA-ID : 2051366
Was this helpful?
What can we do to improve the information ?