Technical FAQs

Ask a Question

What is included in a HOM24M100VP?

Issue:
What is included  in a HOM24M100VP?

Product Line:
Homeline Load Centers

Environment:
Homeline Value Pack

Cause:
What is included  in a HOM24M100VP?

Resolution:
It consists of a HOM24M100C 24 space factory installed QOM100VH main circuit breaker load center. (3) HOM120 single pole 20Amp, (2) HOM230 two pole 30Amp circuit breakers.


CTA-ID : 2051474
Was this helpful?
What can we do to improve the information ?