Technical FAQs

Ask a Question

Is the Canadian, QO QwikPak, catalog number QP60200 UL listed?

Issue:
Product Codes and Standards Listing

Product Line:
QO Load centers

Cause:
Product Listing

Resolution:
No. The load center used in this QwikPak, is not listed for use in the United States and does not have a UL label. Square D does offer a UL Listed QO load center with 60spaces or 60 circuits, for catalog numbers see the current US On-Line digest.


CTA-ID : 2051301
Was this helpful?
What can we do to improve the information ?