Technical FAQs

Ask a Question

When using a HOMCRBGK1 generator interlock kit, where in the panel will the generator back-fed breaker be mounted?

Product features

Product Line:
QO load centers

The back-fed generator breaker will be mounted in positions #2 and #4. REFER TO THE INSTRUCTION SHEETS FOR THE GENERATOR KIT.

CTA-ID : 2051136
Was this helpful?
What can we do to improve the information ?